HOFFMAN ESTATES, IL, October 31, 2019 – Omron Automation Americas, a global leader in end-to-end industrial automation solutions, launched its new E3AS Series Reflective-Type Photoelectric Sensors that combine accurate detection for diverse targets, exceptional sensing distance, environmental robustness, and compact size. These sensors are designed to help manufacturers manage varied and flexible production needs more effectively.

Manufacturers are producing a broader range of products with shorter life cycles, making part detection a dynamic challenge. By maintaining stable detection without being influenced by varying sensing distances, colors, materials, or surfaces, the E3AS sensors make selection, adjustment, and maintenance tasks easier than ever, improving commissioning and operation rates.

The E3AS family’s sensing distance of 1,500mm is five times longer than that of previous models, and the full sensing range of 50mm to 1,500mm eliminates the need for manufacturers to select different sensors for each application. The time-of-flight (TOF) detection method ensures high detection stability regardless of the characteristics of target objects, making sensor selection and adjustment easier than ever.

In addition, the use an antifouling coating on the sensing surface reduces false detection and minimizes maintenance needs in environments with oil, dust, or steam. Dirty sensing surfaces can result in false detections when conventional photoelectric sensors are used, causing unexpected recovery work after line stoppages and periodic cleanings to prevent future stoppages.

Industry professionals interested in learning more about the new sensor family are encouraged to visit the E3AS-F and E3AS-L product pages at the links below.

About Omron Automation

Omron Automation is an industrial automation partner that creates, sells and services fully integrated automation solutions that include sensing, control, safety, vision, motion, robotics and more. Established in 1933 and currently headed by President Yoshihito Yamada, Omron’s 36,000 employees help businesses solve problems with creativity in more than 110 countries. Learn more at http://automation.omron.com/.

Media contact:

Maggie Liu, Marketing Specialist

Omron Automation Americas

maggie.liu@omron.com

847.285.7122