Omron HD-1500 Series Mobile Robot
Introducing the HD-1500. Our Strongest Mobile Robot.
You are currently viewing the HD-1500 Mobile Robot Product Launch page.
HOFFMAN ESTATES, IL, July 21, 2020 – Omron Automation Americas, a global leader in mobile robotics and other advanced industrial automation solutions, recently launched the HD-1500 mobile robot that can handle bulky objects weighing up to 1500kg. This addition to Omron’s robotics portfolio comes after the LD-250 mobile robot launch and further expands manufacturers’ options for autonomous material transport.
Manufacturers are facing a growing need to automate their material handling operations due to an industrial demand for increased productivity and flexibility coinciding with challenges in finding and properly utilizing skilled workers. Social distancing requirements implemented in response to the COVID-19 epidemic further complicate the difficulty of relying on the manual completion of these types of tasks. Mobile robots help fast-paced manufacturing environments maintain speed and flexibility amid these challenges.
The robots automatically calculate the best route for material transportation while navigating safely around people and obstacles without requiring magnetic floor tapes or other guides. This makes them an effective solution for companies seeking to improve flexibility and maximize floor layout options. Omron’s Fleet Manager software controls up to 100 mobile robots of different sizes, configurations and payload capacities, so customers can use the HD-1500 together with the LD-60, LD-90 and LD-250 robots under one system.
The HD-1500’s powerful structure makes it well-suited for industries in which transporting heavy items like car chassis and voluminous pallets is required. By handling some of the transport tasks that would otherwise require a forklift, the new robots also help minimize sources of risk for employees, since forklifts can lead to serious accidents. The HD-1500 offers 360° safety coverage to promote a collaborative and safe working space, and the stop position accuracy of the Cell Alignment Positioning System (CAPS) has also been improved. It even has an onboard, user-accessible Omron PLC.
Industry professionals interested in learning more about the HD-1500 are encouraged to visit the product page at the link below.
Industrial automation partner that creates, sells and services fully integrated automation solutions that include sensing, control, safety, vision, motion, robotics and more. Established in 1933 and currently headed by President Yoshihito Yamada, Omron's about 30,000 employees help businesses solve problems with creativity in more than 110 countries. Learn more at http://automation.omron.com/.
Maggie Liu, Marketing Specialist
Omron Automation Americas
maggie.liu@omron.com
847.285.7122