This application uses a combination of a Function Block Library for the Sysmac controllers and two TM Collaborative Robots using the Listen Node functionality to coordinate the motion of the collaborative robots. The example Sysmac project file can be used as a starting point to add additional logic to handle other tasks that would require the coordination of two (or potentially more) collaborative robots in one work space.

Industries: Any, Auto, Digital

Applications: Assembly, Handling

Innovative Application Tags: Integrated

Return to Applications