This is a dedicated line which incorporates transport of the packs, aggregating different product types and formats, and automatically placing them in different packing cases.

The key issue is that the packs containing different tea flavours – each coming from a different line – must be accurately placed into separate cases for despatch. So when the different teas arrive at the Mespic end-of-line plant, they are first scanned by an Omron FQ vision system, which identifies the different product types. finally, a second Omron FQ-CR vision system reads the code printed on the case, to identify the contents and ensure accurate despatch.

The data is sent via an Ethernet link to the pick-and-place system, which puts the tea packs into different cases. The open cases are first marked with a Data Matrix code, and then automatically sealed.