NJ Series Machine Automation Controller Datasheet
Controller that covers functions and high-speed processing required for machine control and safety, reliability and maintainability.
You are currently viewing the Why Omron’s new SECS/GEM-compliant solutions are beneficial for semiconductor manufacturers page.
As a trusted partner in automation solutions for the semiconductor industry, Omron is committed to providing highly innovative technologies that also meet SECS/GEM requirements. Let’s take a look at the purpose behind SECS/GEM and the ways in which these solutions will benefit semiconductor manufacturers.
SECS/GEM describes how semiconductor manufacturing equipment is supposed to communicate with the manufacturing execution system, or MES for short. Within the standard, the MES is often referred to as the “host.” SECS defines the contents of messages, while the General Equipment Model (E30) or GEM is a higher-layer protocol that defines the messages themselves.
The GEM standard is limited to defining the behavior of the semiconductor equipment as viewed through a communications link. The SEMI E5 (SECS-II) standard provides the definition of messages and related data items exchanged between the host and equipment. The GEM standard defines which SECS-II messages should be used, in what situations, and what the resulting activity should be.
The SECS/GEM standard describes two-way communications through a network or serial cable connection that is independent of any operating system or programming language. Typically, the host side of a connection will be executing on a computer system provided by the factory, while the equipment side runs on a controller provided by the OEM.
By defining messages, state machines, and scenarios, SECS/GEM allows factory software to control and monitor manufacturing equipment. It facilitates true interoperability and can be applied to virtually any manufacturing equipment in any industry.
Demand for SECS/GEM-compliant solutions is driven by semiconductor production, consumer interest in electronic products, and corporate spending on information technology. This area of manufacturing involves some of the most challenging and complicated production systems, and these involve significant capital investment and advanced technologies.
Automation and integration are the keys to success in modern semiconductor manufacturing. Process automation is critical for ensuring the quality and throughput of process sequences and corresponding parameter settings, as well as integrating all fabrication activities to provide the requisite efficiency, reliability, and availability.
Many companies are under pressure to innovate without capital expenditure in a tight currency market, so a top driver for SECS/GEM solutions includes companies looking to retrofit equipment and improve quality.
Common applications in front-end manufacturing include:
Common applications in back-end processes include:
Our NJ Machine Automation Controller with SECS/GEM functionality provides direct communication to the Host PC in a single platform controller, complete with embedded EtherCAT for real time I/O, motion, vision, and safety. Furthermore, the NJ501-1340 supports the V640 RFID system used for tracking FOUPs (wafer carriers).
The following products are available for use with the NJ SECS/GEM: