E2EW Weld Field Immune Metal Faced Proximity Sensor
Long range metal face inductive proximity sensors with equal sensing for aluminum and iron
You are currently viewing the How IO-Link improves predictive maintenance and speeds up sensor reconfiguration page.
Smarter sensors mean better insights into what’s really going on at the machine level, and these insights lead to better decision-making and less downtime. Setup, predictive maintenance, and reconfiguration are all great ways to use IO-Link. Let’s take a look at what IO-Link is and how you can use this powerful protocol in your applications.
IO-Link is an open-network point-to-point communications protocol. IO-Link-enabled sensors communicate to master devices through IO-Link based on a certain standard, and from there on, they’re open-network to whatever fieldbus protocol you’re using. The international standard used by IO-Link is IEC 61131-9.
IO-Link allows you to pull a greater variety of information out of discrete sensors that would normally just tell you whether they’re on or off. The protocol was started by a consortium of different companies involved in automation who wanted a standard, open-network solution for getting more information out of I/O spread throughout the factory floor.
Lots of early IO-Link adopters found value in the protocol for real-time condition monitoring and predictive maintenance. If you’re operating in a weld environment, for example, and slag is starting to cake onto your proximity sensor, the IO-Link functionality can tell you the detection strength so the sensor can be cleaned before the slag causes false trips.
If you’ve got dozens of sensors on your line, and you’re starting to notice a sensor-related quality issue, using IO-Link means that you don’t need to stop the line and inspect each sensor individually. A quick check will tell you which I/O port has a down sensor on it.
Trying to reduce downtime in your plant?
Given the market pressures driving manufacturing today, many facilities are producing multiple different parts on the same production line. This creates a need for scalable technologies that support faster changeovers. IO-Link addresses this need by speeding up sensor reconfiguration and helping a smaller team do more with their time.
With some of our newer IO-Link sensors, you can set different levels that you want them to output at. If one sensor gets broken, you simply replace it, and your IO-Link master can push the configuration to that sensor. You don’t have to waste a bunch of time reconfiguring the whole thing.
Want to start gathering more meaningful data from your sensors?
Long range metal face inductive proximity sensors with equal sensing for aluminum and iron
Small diameter proximity sensors for space constrained applications
DC 2-wire inductive proximity sensors that offer 1x and 3x sensing ranges
The NEXT generation in enhanced sensing
A new family to our E3AS line that incorporates CMOS technology into a small package.
Time of flight photoelectric sensor in 316 SUS or plastic housing
Next-Generation Distance-Settable Compact Background Suppression Sensors
Compact plastic laser photoelectric sensors with multiple sensing modes
Many applications in the life sciences, food and commodity, and other industries require small-form-factor smart cameras to be embedded within a machine. Understandably, OEMs with such needs are looki...
Blow molding is an essential process within the packaging industry that is used to create hollow plastic parts like plastic bottles. After raw plastic is heated, it gets turned into a parison, which i...
As machines become more connected, the need to service equipment remotely is escalating. Production is often running 24/7 and manufacturers expect immediate action from machine specialists. Not having...
One of the easiest ways for manufacturers to transform their operations with IIoT capability is to use IO-Link. This internationally accepted platform allows sensors to go beyond a simple ON/OFF readi...