40 Years in Vision
We've invested in vision solutions for four decades, in addition to 80 years of innovation in industrial automation.
You are currently viewing the Machine Vision page.
Omron's comprehensive machine vision hardware line includes industrial cameras, vision systems and smart and PC-based cameras that are scalable across software platforms. Our portfolio offers compact form factors for tight spaces, high-speed imaging for fast-moving production lines, and high resolutions for detailed inspection.
As the market's only total solution provider, we combine our cameras with a powerful software platform that's fully integrated with our controllers and robotic solutions and also works well with third-party devices.
We've invested in vision solutions for four decades, in addition to 80 years of innovation in industrial automation.
We're among the biggest players in vision solutions and industrial barcode scanning.
We're the only factory automation vendor that can provide a fully integrated solution, including cameras, input, logic, output, robot and safety devices.
The F440 is the latest in high-resolution compact smart cameras from Omron Automation. Featuring a 5 MP Global Shutter sensor, this fully contained vision system can tackle even the most difficult of ...
The next gen of the popular MV-40 model, featuring the smallest IP65/67-rated, true-industrial Ethernet smart camera now with expanded functionality.
Omron FHV7 cameras features the world's first multi-color light and high-res image sensors. It brings the power of a vision system to a smart camera.
The fast and most flexible vision system with newly added AI Components to the already complete and powerful set of inspection tools.
Ready to deploy single programmable devices that are capable to acquire an image, process that image and provide an output/judgement to the machine.
Robust and powerfull Vision controllers that can operate with single or multiple cameras connected to it. The cameras acquire the images and send them back to the vision controller for analysis and an output/judgment.
GigE based custom cameras and dedicated Vision Application Software license with the flexiblity to install it on your own IPC.
Industrial cameras with multiple interfaces that could be applied to a variety of applications, including just displaying a live image or analyzing it with a vision software application.
Software for smart cameras, vision systems and PC-based cameras.
By combining barcode reading and inspection tasks into a single device, the MicroHAWK platform offers manufacturers greater flexibility in production line layouts, cuts hardware-related costs and dramatically reduces wiring and maintenance work.
Why use multiple devices when a single camera can do it all?
Learn more about machine vision and smart cameras
Machine vision is the automatic extraction of information from digital images. A typical environment would be a manufacturing production line where hundreds of products are flowing down the line in front of a smart camera. Manufacturers use vision systems instead of human inspectors because it’s faster, more consistent and doesn’t get tired. The camera captures the digital image and analyzes it against a pre-defined set of criteria. If the criteria are met, the object can proceed. If not, the object will be re-routed off the production line for further inspection.
For example, a beverage manufacturer would typically have human inspectors watching thousands of bottles move down a production line. The workers would need to ensure every bottle cap was secured correctly, every label was on straight and contained the correct information and every bottle was filled to the appropriate level. With machine vision, this entire repetitive process can be automated.
Vision solutions are used heavily in conjunction with robots to increase their effectiveness and overall value for the business. These types of robots resemble a human arm with a camera mounted at the “hand” position. The camera acts as the robot’s “eyes,” guiding it to complete the assigned task.
A vision system has five key components that can be configured either as separate components or integrated into a single smart camera. The correct configuration depends on the application and its complexity. The five key components are:
There are four main benefits:: reducing errors, increasing yield, track parts and products as well as comply with regulations.
Cameras for inspection ensure fewer bad parts enter the market which can cause costly recalls and tarnish a company’s reputation.
Prevent mislabeled products whose label doesn’t match the content. These defects create unhappy customers, have a negative impact on your brand reputation, and pose a serious safety risk – especially with pharmaceutical products and food items for customers with allergies.
Turn additional available material into a saleable product.
Avoid scrapping expensive materials and rebuilding parts.
Reduce downtime by detecting product routing errors that can cause system disruptions.
Uniquely identify products so they can be tracked and traced throughout the manufacturing process.
Identify all pieces in the process, reducing stock and ensuring the product will be more readily available for just-in-time (JIT) processes.
Avoid component shortages, reduce inventory, and shorten delivery time.
To compete in some markets, manufacturers must comply with various regulations.
In pharmaceuticals, a highly regulated industry, machine vision is used to ensure product integrity and safety by complying with government regulations such as 21CFR Part 11 and GS1 data standards.
Machine vision is better-suited to repetitive inspection tasks in industrial processes than human inspectors. Machine vision systems are faster, more consistent, and work for a longer period of time than human inspectors, reducing defects, increasing yield, tracking parts and products, and facilitating compliance with government regulations to help companies save money and increase profitability.
A common machine vision application is automated measurement. After an image of a part is captured, the software compares the measurement to a required tolerance. For example, in factory automation, machine vision systems are used to measure the gap in a spark plug, ensuring it meets the tolerance required to function properly. In the packaging and labeling industry, machine vision is used to measure the fill level of a water bottle, ensuring it was filled to the correct height.
Another common machine vision application is counting – looking for a specific number of parts or features on a part to verify that it was manufactured correctly. In the electronics manufacturing industry, for example, machine vision is used to count various features of printed circuit boards (PCBs) to ensure that no component or step was missed in production.
Machine vision can be used to locate the position and orientation of a part and to verify proper assembly within specific tolerances. Location can identify a part for inspection with other machine vision tools, and it can also be trained to search for a unique pattern to identify a specific part. In the life sciences and medical industries, machine vision can locate test tube caps for further evaluation, such as cap presence, cap color, and measurement to ensure correct cap position.
Machine vision can be used to decode linear, stacked, and 2D symbologies. It can also be used for optical character recognition (OCR), which is simultaneously human- and machine-readable. In factory automation, machine vision is used to sort products on a production line by decoding the symbol on the product. The symbols themselves can also be verified by machine vision-based verification systems to ensure that they comply with the requirements of various symbology standards organizations.
The most common reasons to consider when selecting a smart camera include:
The most common reasons to consider when selecting a vision system include:
The most common reasons to consider when selecting PC-based cameras include:
The most common reasons to consider when selecting PC-based vision cameras/industrial cameras include:
The Lens Selection Tool allows you to quickly find a standard, vibration/shock-resistant or telecentric lens for Omron vision systems or smart cameras. Provide the camera distance or field-of-view requirement, and a short list of lens options will appear. Creating a bill of materials has never been easier.
The extensive capabilities of machine vision boil down to just a few fundamental functions -- location, measurement, counting and decoding. They depend on the common capabilities of recognizing pixel intensity values, finding edges contours, and matching shapes and patterns. This white paper looks at each foundational task in greater detail.
Omron helps manufacturers drive down costs, automate critical manufacturing processes and increase yields through data acquisition and control solutions. We offer versatile decoding power within the world’s smallest industrial barcode readers. With the highest-performance imaging engine in its class, MicroHAWK readers offer modular hardware options to take on any decoding task.