E2E NEXT DC 3-wire Best-in-Class Proximity Sensor
The NEXT generation in enhanced sensing
You are currently viewing the Get to know our top three trends in sensor innovation page.
Although there are many different ways to make progress in sensing technology, we place a premium on three key areas of innovation: smarter sensors, longer sensing distances, and robust, IP-rated technology. Let’s take a look at each in turn.
Did you know that sensors can now offer more data besides a simple ON/OFF reading? As we continue to expand our already broad sensing portfolio, we’re finding ways to incorporate IO-Link functionality so that users can access the data they need for real-time condition monitoring and better predictive maintenance.
IO-Link lets you pull more data from discrete sensors. If you’re using photoelectric sensors in a weld environment, you’ll be able to see when their light intensity dips below a certain level, indicating lens occlusion. IO-Link-enabled sensors utilize the same internal components as traditional sensors, so access to this additional information comes at no additional cost.
Long sensing distances are very important for maximizing uptime. When sensors are farther away from the targets, they’re less likely to get damaged. We’re always striving to achieve stable detection at industry-leasing sensing distances.
Having the option to increase sensing distances is also great for flexibility, since it enables the use of smaller form factor sensors for the same applications and helps address size and layout constraints. Our E2E NEXT proximity sensors, for example, have an exceptionally long sensing distance and are ideal for flexible manufacturing. (They also have IO-Link.)
There’s a lot going on in a typical manufacturing environment, and there are lots of ways that sensors could get damaged. Corrosive chemicals of various types are common in food and beverage washdown environments, while automotive plants feature grease, dust, cutting oil, and weld slag. If any of these things can easily damage your sensors, that’s a big problem.
Fortunately, automation industry leaders like Omron are addressing this issue by designing sensors with high IP ratings that protect against dust and water ingress. Additionally, many Omron sensors are resistant to cutting oil, which is very important given that approximately 30% of unexpected component failures can be traced back to cutting oil.
Interested in learning more about Omron’s trends in sensor innovation?
The NEXT generation in enhanced sensing
Small diameter proximity sensors for space constrained applications
Proximity Sensor with Threaded Nickel Plated Brass Long Barrel Housing
DC 2-wire inductive proximity sensors that offer 1x and 3x sensing ranges
Many applications in the life sciences, food and commodity, and other industries require small-form-factor smart cameras to be embedded within a machine. Understandably, OEMs with such needs are looki...
One of the easiest ways for manufacturers to transform their operations with IIoT capability is to use IO-Link. This internationally accepted platform allows sensors to go beyond a simple ON/OFF readi...
One of Omron’s main focuses with respect to sensor innovation is to incorporate more “intelligence” — that is to say, more ways to gather meaningful data — into our latest sensor lines.
IO-Link technology was created in response to three consecutive challenges. The first was the tendency of manufacturers to use whichever I/O system protocol they liked best, causing their devices to n...