Let’s discuss how the latest handheld barcode reader is helping manufacturers to easily overcome these traceability challenges.
Just click and read
Most industrial handheld barcode readers lack the ability to automatically adjust settings to instantly read different types of barcodes at different distances. Users often need multiple readers and complicated reprogramming to do this. With the V460 there is no need to purchase multiple units. The barcode reader comes native with a predictive autofocus feature, allowing it to automatically adjust to different sizes, surfaces, and types of barcodes.
Automatic selection of optimal lighting
Specialized lighting and algorithms are often required to read direct part marks on challenging surfaces. The V460 is equipped with patented pending intelligent lighting that allows the user to read any type of barcode with the automatic selection of high powered, multi-axis, multi-colored lighting. This feature enables the barcode reader to automatically select the most suitable type and color of lighting to the type of barcode that is presented.
Quick setup to easily communicate data
Most handheld barcode readers require costly and complex traceability setup. The V460 offers a built-in Power over Ethernet port, a single Ethernet cable connection for power and communication and fieldbus connectivity. Users save time and integration cost with its simple connectivity and pre-built function blocks for the etherNET & fieldbus communications.
Built to last in the harsh manufacturing environments
This rugged handheld is designed for long life in industrial situations. It is built to withstand the harsh treatment of the manufacturing environment. Its durability reduces hardware maintenance and replacement costs.
Related Resource
V460-H Industrial Handheld Barcode Reader Communication Manual
Intelligent Barcode Reader for Direct Part Marks and Labels
An intuitive out-of-box reading experience, as well as seamless PLC connectivity. Its durable and long-lasting body ensures reliable performance in industrial environments.